Dear Sir/Madam
I have used bq76920 just to monitor cell voltage of 4 cell connected in series. But while interfacing with arduino nano using i2c communication only two cell voltage I have able to read. other cell voltage is coming as '0'. I was unable to find the root cause for this. Also I have checked by replacing the IC with other IC.I have done the connection diagram according to Data sheet. The following pins are only used 3,4,5,9,10,12,13,14,15,16 and 17. Please suggest if i have missed any pin just to monitor cell voltage.