This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92602-Q1: 2.5A/per channel

Part Number: TPS92602-Q1

Hello

            Does TPS92602 support below condition ? especially 2.5A per channel output current and 86KHz PWM dimming frequency. Thank you. 

Vin: 12V

Vout : 24V

Iout: 2.5A/per channel

PWM dimming frequency: 86KHz

BR

Patrick

  • Hi Patrick,


    2.5A output current is ok for TPS92602-Q1. Just make sure the whole system design can meet the current spec.
    For the PWM dimming frequency, actually 86kHz is quite high for the device, because the switching frequency is just several times of the PWM frequency. The PWM dimming accuracy won't be very good, especially when the dutycycle is very high or very low. May I ask why so high PWM frequency is needed?


    Best Regards,
    Shirley He
  • Hi, Patrick,

    I'll close this thread due to inactivity and if you have more questions please reply to it directly and it will open again.

    Please help to click "Resolve" if the problem is solved.

    Thanks.
    Regards,
    Kenneth