Part Number: LM5041A
Hi, I'm an engineer of hardware, and I'm encountering a problem in using LM5041A, and the phenomenon is : when the temperature going up, the HD's PWM become a little larger , but the CS waveform is the same, the COMP pin's voltage is fewer ( FB is connected to gnd). Is this the IC's internal problem ? for I don't know why the COMP pin's voltage is fewer (200 mV lower from 31 degree to 100 degree) the HD's PWM is larger(1.8% larger, the CS pin's voltage is almost the same)