This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25601: bq25601 / Disable temperature monitoring function

Part Number: BQ25601

Hi,

I know that the recommended method to disable temperature monitoring function is to pull up and down TS pin with 10kohm so the additional two resistors are needed. Now the customer consider bq25601 but their board has only limited mounting area, so they would like to disable it by adding only one external component or no additional components.

Do you have any idea to disable it with reduced component? I understand it need to apply the voltage that is between VT2 and VT3.

Best Regards,
Satoshi / Japan Disty