Hello I'm designing a circuit using the TPS61220 and I have an input voltage of 2.75V at the Vdd pin. I'm wondering what will happen if I drive the enable pin at a higher logic say 5V when it is a couple of volts higher that the Vdd of the part. Will this damage the chip in any way? I didn't see a maximum for the Ven pin with respect to the Vin pin.