This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EM1402EVM: find part number for battery pack

Part Number: EM1402EVM

i got 1402EVM. But not include battery cases or barttery pack PCB.

like below link.

http://www.ti.com/tool/TIDM-TMS570BMS

anybody could tell me the battery model name ?

  • Hi John,

    This is just a demo setup with the EM1402 EVM and the TMS570 Launchpad. The actual cells and PCB are not part of the demo.


    The cells are typical lithium ion cells (3.6V nominal, 4.2V charge, 2200mAh I believe). You can find them online or from your local cell vendor.