This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

wide input range single channel white LED string driver

Other Parts Discussed in Thread: TPS92692

I need to drive from 10 to 16 white LEDs from a constant current source in the range of 20 to 40mA.  The input voltage range must be 12V to 24V.

I have been searching but have not found a suitable buck/boost driver.  Can anyone suggest a single IC solution for this function?  If not, any other suggestions are appreciated.

Thanks for any help!

  • Hello,

    Does this need to be a buck-boost or will a boost work. Vout minimum should be around 30V. If you dim the boost may not work. As for a buck boost the TPS92692 should work though the current sense resistor would need to move to the LED- to prevent exceeding the pin ratings. Also if a series P-FET is needed that would have to be level shifted.

    Regards,