Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ34Z100, , BQSTUDIO
Good morning,
after completing the learning cycle accordingly to SLUA597, it is not clear how to create a golden file ready to be used in production.
In SLUA334B it seems the "Update Status" parameter must be manually changed from 06 to 02. In SLUA664 (referred to BQ34Z100 instead of BQ34Z100-G1), I can read: "When the golden DFI file is created by bqEASY, bit 2 will be cleared, leaving Update Status=0x02. Note that none of these bits should be manually changed."
So I don't know if and how to change the Update Status from 06 value (at the end of the learning cycle) to 02 (value suitable for production programming of the BQ34Z100-G1).
Is there any detailed procedure description for extracting the golden file at the end of the learning cycle by using the BQ Studio software?
Thank you and best regards
Matteo