Hi,Team:
Can you help to check if TPS54388 has eco mode? Seems not but no detailed explain in datasheet.
From datasheet, there is boot-PH >2.2V requirement. If it has ECO mode, it may have some issue in low dropout and light load condition for example Vin=5V, Vout=3.3V,Iload<1mA or even no load.
Besides, what's the start up delay from Enable rising edge to Vout rising? From datasheet figure 28, seems there is 0.2-0.4mS delay. Now, we have application that need the very short enable to Vout ready time and need to check.
The TPS54388-Q1 design improves dropout by operating at 100% duty cycle as long as the BOOT-to-PH pin
voltage is greater than 2.2 V. A UVLO circuit turns off the high-side MOSFET, allowing for the low-side MOSFET
to conduct when the voltage from BOOT to PH drops below 2.2 V. Because the supply current sourced from the
BOOT pin is low, the high-side MOSFET can remain on for more switching cycles than are required to refresh
the capacitor. Thus, the effective duty cycle of the switching regulator is high.