This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SM72442: request DC/DC for solar inverter.

Part Number: SM72442

Hello TI,

My customer is looking for DCDC(Buck-Boost) solution including MPPT feature. We are reviewing SM3320EVM but it couldn't meet Power requirements. 

Could you please recommend suitable solution with part number and software?

Input Voltage from Solar Panel : 10Vdc ~ 80Vdc

Output Voltage (for Battery charging) : 12V, 24V, 48V

Output Power: 1KW

Best regards,

Downey