This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM84205: TPSM84205

Part Number: TPSM84205


Dear Sir or Madame,

the module: TPSM84205, could it source and sink the output current and maintain the output voltage stability?

I have a circuit with few power rails (5VDC, 12VDC, 24VDC)

one of power rails is powered by 5VDC +/-20%, but the output current is not DC, it sinks and sources from 5V output between -500mA to +500mA

Could I use the TPSM84205 for this power rail?

Could the TPSM84205 sink and source +/-500mA maintaining the output voltage stability?

Best regards

Nikola