This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28C43: Transformer Design

Part Number: UCC28C43

Hi,

I am designing a 48V isolated Buck-Boost Converter from UCC28C43D.

Input range ( 36V-75V DC).

Isolated output 48V-DC.

Current Requirement: 2A.

When I enter these requirements on webench, It asks me to design a custom transformer. 

Can someone help with, How to design a transformer for requires specifications?  Webench suggests me the Core and Bobbin for transformer but it is not available on digikey. Even if I get those, where to find the winding material and how to wind it?

Thanks 

Vishal Kakade

R&D Engineer

Logic-Fruit Technologies.