Other Parts Discussed in Thread: BQSTUDIO, EV2400
I use RL78-MCU to communicate with the PCB board on which BQ40Z50-R1 is mounted, but some boards always return incorrect data.
Even if bqStudio is started, "Target Selection Wizard" is displayed on board which returns incorrect data and it is not recognized automatically.If you try with a normal board, the BQ40Z50-R1 will be recognized automatically.
The cell is not connected and voltage is applied to the PACK terminal side.
We know that it is possible to communicate properly by replacing the BQ40Z50-R1, so we suspect a device failure.
I upload communication contents when bqStudio starts up.
Do you know the cause?
Thanks.
normal
Bus Definition: I2C | |||||
Time | Repeat Start | Direction | Address | Data | Missing Ack |
1.39E-17 | Write | 16 | 22 3E | X | |
2.60E-02 | Write | 16 | 20 3E | X | |
5.10E-02 | Write | 16 | 22 3E | X | |
1.83E-01 | Write | 16 | 2F | ||
1.84E-01 | X | Read | 17 | 0B 45 00 01 06 00 24 00 03 85 02 00 D0 |
error
Bus Definition: I2C | |||||
Time | Repeat Start | Direction | Address | Data | Missing Ack |
1.39E-17 | Write | 16 | 22 3E 00 00 | X | |
2.60E-02 | Write | 16 | 20 3E | X | |
5.20E-02 | Write | 16 | 22 3E 00 00 | X | |
1.74E-01 | Write | 16 | 2F | X | |
1.84E-01 | Write | 16 | 00 01 00 06 | ||
2.05E-01 | Write | 16 | 0 | ||
2.06E-01 | X | Read | 17 | 17 17 17 | |
2.14E-01 | Write | 16 | 00 02 00 39 | ||
2.36E-01 | Write | 16 | 0 | ||
2.37E-01 | X | Read | 17 | 17 17 17 | |
2.45E-01 | Write | 16 | 00 00 00 13 |