Other Parts Discussed in Thread: GPCCEDV
I configured the bq78530 as follows:
AFE Cell Map :0x1F (My pack has five Li-ion cells)
Design Capacity mAh :11000
Design Capacity cAh: :4070
Design Voltage :3700
Learn Full Charged Capacity :11000.
I applied 1.6A load to bq78350.
After a period of time, the remaining capacity suddenly drops form 75% to 7%.
And I charged the cells to 21V, the remaining capacity is only 16%.
I think the capacity should derement two in about 1 second. But the remaining capacity decrement one in about two seconds.
I seems the gauge don't cares about cell numbers. Does Design Capacity mean a single-cell capacity?
I don't konw why does the problem happen.