This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28063: Apply 10KΩ to PHB

Part Number: UCC28063

hi

PHB is basically connected to VREF and 0 ohm.

Is there any part that affects circuit operation when this part is connected with 10k ohm?

Can this affect the Impulse test?