This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54162-Q1: Mission profile confirmation

Part Number: TPS54162-Q1

Hi,

We are using  TPS54162QPWPRQ1 in one of our application and wants to confirm whether HTOL test done by TI covers the below mission profile or not?

 Mission profile :

Maximum Power dissipation: 450mW

Junction temperature rise above ECU internal ambient temp: 11 °C

 

ECU External ambient temperature.

ECU internal ambient Temperature

Duration of ECU exposure to the given temperature

[h]

Temperature distribution

[%]

-40 °C

-27 °C

1500 h

6 %

23 °C

36°C 

16250 h

65 %

60 °C

73 °C

5000 h

20 %

70 °C

83 °C

2000 h

8 %

85 °C

98 °C

250 h

1 %

Sum:

25000 h

100 %

 

Tj would be 24 degree high with respect to ECU External ambient temperature.