Hello TI Experts,
I am evaluating BQ76PL455 now and have below doults need your help:
1.The isolation must be two sides like ADUM5402? Can I use one side ADUM2402?
But if I use isolation like ADUM2402,when BQ76PL455 is in shutdown mode,their will be no input voltage to ADUM2402,the BQ76PL455 cannot be woke up~
So must I use isolations like ADUM5402? So what's the function of NPN? Is it necessary to use NPN?
2.Is it necessary to put an inverter between BQ76PL455's Wake up pin and Isolation?Can I know why? I see their's somebody do like this but I have no idea why to do it~