This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3-phase TR rectifier I/O controller EVM board

Hi there,

 

I have been back to high power design.

My system contains 3phase, 380V, 50Hz  ac input, secondary surge protector, Aux Tr ( single phase, 380V/220V, 300VA), phase transformer( 3ph, 380v/12v,0v,12v,100VA) and a main transformer ( 3ph, 380V/9V,18V,800VA),

SCR(1600V, 50A) bridge, DC reactor( DC 20V,20A). Rectifier output should be DC 20V 20A.

 

My requested EVM should be,

 

1. PTR secondary windings  phase, amplitude and rating controller.

2. MTRs secondary fuse (690V, 32 A)  sensing 

3. SCRs switching controller.

4. 50mlV, 30A shunt sensing,

5. GPS communication,

6. RSM 

7. LAN

8. Display....etc,

 

 

Kindly recommend me one.

You can also transfer this post to suitable forum.

 

Regards

Hasan