Hi
Is it OK to connect PowerPad to PGND on the other layer with through-hole for heat dissipation?
We don't use ethernet input but adapter input is used. Only PGND has large pattern.
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi na na78,
The dissipation is mainly for the internal pass FET of the PD controller (from PoE). Since Ethernet input is not used the pass FET is not dissipating but it doesn't hurt to connect the pad to a plane of copper for some extra mechanical stability. However, I would put it on a floating plane and not PGND since if not designed correctly, the adapter on VDD-RTN, with VSS and RTN shorted will place a voltage on VDD-VSS and might turn on circuitry on the PoE (VSS) side.
Regards,
Darwin