Tool/software: WEBENCH® Design Tools
I am using Webench power designer and I am finding it extremely frustrating that I can not go into a schematic design and change the load resistance value. Well I can, but there are arbitrary limits set by the tool which it does not seem possible to change. I am investigating an issue with a DC-DC converter where I know I have problems and I want to explore the limits. In particular I want to look at the Bode plots and determine how close I am to stability in the design.
The design is a DC-DC converter generating 48 V from 12 V with an output current range from 5 mA to 125 mA. I have a design which sources 5 mA and I want to now increase the current to 15 mA. I cannot edit the Rload value on the existing design and if I try to create a new design and change the component values to those I have in the 5 mA design, when I come to edit the compensation capacitors the tool is not allowing me to set the values I want. I suspect that this is because the value will make the design unstable and the tool is trying to be helpful and not allowing me to do it.
The tool is powerful but does not have enough flexibility to enable me to explore the design space.