Hi,
My customer has a question.
Q.
Datasheet Page 5. In 6.5 Electrical Characteristics,
IEN TEST CONDITIONS is VIN = 4 V to 36 V, VEN = 36 V.
Datasheet Page 4. 6.1 In Absolute Maximum Ratings,
The rating of EN is VIN + 0.3V.
The condition of Vin = 4 V and VEN = 36 V,
Have not exceeded maximum ratings?
Best regards,
watanabe