Hi
My customer has question.
Is it possible to use LP 8860 in "Direct PWM Mode" + "Hybrid Dimming"?
The customer wants to do LED dimming frequency at 200 Hz.
⇒ We believe it is possible for Direct PWM Mode.
However, the resolution of customer's "PWM Input" is 0.1% (1000: 1) is the limit.
In contrast, the required SPEC is 0.02% (5000: 1).
Customers want to consider whether they can be realized by "Direct PWM Mode" + "Hybrid Dimming" to satisfy this.
Is it possible?
Best Regard
T Kishi