Other Parts Discussed in Thread: TPS53625
Hi
Recently I used TPS53625 as my x86(ATOM C3000) CPU VR chip. I set the TPS53625 min Vcs(ocp) value to 4.5mV. When I run linux on the CPU.I found the running speed is very slow. I use dd command the write sata disk for testing the performance of the CPU, write 1GB file, the speed is 22MB/s。 Then I found when I set the Vcs(ocp) value to 36.7mV. The performance of CPU increased obviously. The same sata disk write test for 112MB/s speed. I am confused. why the Vcs(ocp) setting can make such big influence on CPU performance? the TPS53625 Icc(max) setting is above the CPU demand current.