This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74610-Q1: disable the T0

Part Number: LM74610-Q1

Hello ,

Is there any solution for avoid or reduce voltage drop at T0 in LM74610-Q1. 

  • Always ON.PPTXHi Hari,

    To avoid the pulsing of the LM74610-Q1,the VCAP voltage needs to be held at >6.3V. This could be done by applying an external isolated power supply across VCAPH and VCAPL. If there is an onboard DC-DC converter then you could even use the circuit in the attachment to create a isolated power supply and connect it across VCAPH and VCAPL. This is basically a voltage double circuit derived out of a switching node of a DC-DC converter.

    Regards,

    Dilip