This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53622: Question about differences between TPS53622 and TPS53622A

Part Number: TPS53622

Why is there no datasheet for TPS53622 on digikey, mouser, and avnet?  Other parts in the TPS536xx line have full datasheets.  Are you discouraging this part in new designs?

It's on my list of most suitable TPS536xx parts for a current design.

Thank you,

Dan

  • Hi, TPS53622 full datasheet would require NDA, so if you can verify the NDA with your company, you can get the full datasheet. To answer your question, the main difference between TPS53622A and TPS53622 is that the tracking OVP of TPS53622A can be programmed as either 200mV or 400mV while TPS53622 is set dynamically based on the Intel protocol selection.