This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54561: Output current trace width

Part Number: TPS54561

This part is supposed to be able to output up to 5A continuously, but the output SW pin only allows a trace that is 0.32mm thick, this is the thickness of the recommended pad size for the IC footprint.  On 2 oz/ft^2 copper, with external trace layers exposed to air, 0.32mm only allows 1.7A.  So, how is this device supposed to be able to output 5A?