Hi Support Team
My Customer has a question regarding the what the minimum capacitance is required for operation on the bq charger. They are having a serious issue getting cap and are being forced by their manufacturer to use smaller sized cap. When using the smaller caps they are finding that the "real effective" capacitance is much smaller than expected due to the voltage coeff. So for example an 0805 10uf cap when switched to a 0605 10uf may be as low as 2uf in their system (with a charging voltage of 12v). This is a very high volume application and they need to understand minimum requirements for stability.
Thanks
Jeff Coletti