Hi Team,
Please see question from my customer below.
I have a question about the bq24166. When I am charging my battery the chip gets really hot (my infrared camera says more than 70°C). This is getting hotter than my wireless charging itself. I need to find a way to reduce temperature of the bq21466. I use the wireless charging as an input source. I measure 6.5V there and the current is about 1.6A (calculated with the help of the WPC input power of my charger). Can you help me and tell me why the bq24166 is getting so hot?
Thanks,
Needhu