Other Parts Discussed in Thread: LM5161
I want to use LM34927 to converter Input voltage 24V to output voltage 12V. The output just to drive the 16pcs relays. Every relay core resistance has 270Ω . So I calculate output current about 711mA . I want so make sure the LM34927 can drive it. I see in the datasheet page 6 showed the current limit threshold minimum is 0.7A when the Vin equally 48V . Can help me make sure below 2 questional.
1. What output current maximum current value when Use the LM34927 to make 24V converter to 12V?
2. If the output current maximum current value can satisfied my design how to decide the output inductance value?
Best regard,
Brian