Hi,
Iam looking for a DC to DC step-up Booster circuit with below voltages with peak current being 30A.
input - 12V or 24V DC
output - anything between 90V to 120V DC.
can i get this in TI or please suggest where can I get.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Iam looking for a DC to DC step-up Booster circuit with below voltages with peak current being 30A.
input - 12V or 24V DC
output - anything between 90V to 120V DC.
can i get this in TI or please suggest where can I get.
Hi Garrett,
I'm planning to use it for Electric bike.
with or without isolation is not a problem.
Thanks for the response and sorry in the delay.
Thank you very much Garrett.
Can you please give me some more details.
Iam open to suggestions on Booster. from your suggestion I understand LM5170 with an external gate driver is good but, Bridge converter is better.
Can you please suggest me, what type of Bridge converter or any specifications of Bridge Converter to be used.