This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS566250: About the default resistance value of TPS566250

Part Number: TPS566250

Hello.

My customer uses TPS566250.
My customer want to set the output voltage to 1 V at default.

Recommended resistance values are listed in Table 6 of the data sheet p.17, but the resistance values of R1 and R2 are all the same value(R1=1.37V/R2=1.65V).
Can I set the output voltage to 1V by default?

Best regards.

Yurie