Product Information
Discrepancy on direction of soldering coils
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Product Information
Discrepancy on direction of soldering coils
Christine:
The dual power inductors identified in the pictures for PTH05010WAH LTC 771738V and 681716V modules may have a different “visual appearance” and markings, but the performance (fit, form, and function) of the power inductor remains unchanged. The mechanical mounting and electrical characteristics are equal when using either vendor power inductor.
1a. Each fully qualified and approved power inductor vendor must meet the TI inductor electrical and mechanical specification. There are no two inductor vendors which have the same manufacturing process. Each Inductor is designed to specific electrical inductance and mechanical size.
Tom
: