This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160: Error loading or running application library: Exception has been thrown by the target of an invocation

Part Number: UCD90160


I'm trying to program UCD90160 with Fusion Digital Power Designer. The older version (v 2.0.159)  couldn't do it properly. So I installed the latest version (v 7.0.25). When running the application I got the following message: 

Error loading or running application library: Exception has been thrown by the target of an invocation

The older version I used (v 2.0.159) doesn't seem to have the problem. Can anyone please help? 

Thanks. 

-Nikko