Part Number: BQ20Z95
Hello TI
We are struggling to understand why the FCC (register 0x16) sometimes reports 0 together with SOC (register 0x0d) reporting 0 although the cell voltage is nearly on full level. The max error (register 0x0c) is '1'.
This happens when the battery pack is put in temperature chamber and going from room temperature to subzero temperatures with no load on battery. (Battery pack is operational down to -40 degree C with a maximum discharge of C/8)
Our vendor for the battery pack with built-in bq20z95 gauge claims that the parameters are correct.
We would like to log different kinds of parameters meanwhile the battery pack is subject for cooling down do subzero temperatures.
In the technical reference (sluu264a) there is not much to get in terms of which resistance grid is used, the DOD when OCV is measured, the time since OCV was measured and updated Qstart and so on.
Are there some undocumentet registers available to be able to read out such parameters?