Other Parts Discussed in Thread: TIDA-01423, , TPS54335A
Hi
I'm referrring TIDA-01423.
http://www.ti.com/lit/ug/tiducy3/tiducy3.pdf
Is it possible to meet following condition using TPS563201?
Input:5V
Output : -2V / 1.5A
My calculation is on table below. If it is correct, TPS563201 can have capability to our requirement.
VOUT | -2 | |
VIN | 5 | |
D | 0.3 | |
Fs | 580 | KHz |
L | 1.5 | uH |
ΔIL | 1.724137931 | |
Ilimit | 3.3 | A |
IL(avg) | 2.437931034 | |
Iout | 1.706551724 |
Could you please go over our estimation?
BestRegards