Other Parts Discussed in Thread: TPS62177
Currently I use a TPS62177 as 3.3V voltage source for my application.
There are applications in which a USB stick is to be connected to the device for various purposes. For this I need a second 5V power source to operate the USB host interface. Is there any argument against feeding the TPS613222A from the TPS62177? The TPS613222A data sheet only lists battery-powered applications.