This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: GPC Reports for CEDV

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQSTUDIO, GASGAUGECHEM-SW,

TI occasionally updates the CHEM ID list for cells that have been characterized.

Is there a place to obtain CEDV GPC reports that already exist, so that the effort already done does not have to be duplicated?

Thanks,

Larry

  • Hi Larry,
    The GPC CEDV file is not really a characterization of the cells but a set of parameters for the pack assembly and conditions. There is not a library of the CEDV parameter files.
    The cell CHEM ID characterization is used primarily for IT gauges, but is also used in the bq78350-R1 for better estimation of capacity on reset. bqStudio will load the selected chemistry to the device. The tool GASGAUGECHEM-SW can be used to update the chem id selections available in bqStudio, use the bqStudio version. You can browse the Chemistry tab in bqStudio. I don't know of a text list or report to browse separate from the tool.
  • Thanks for the response.