Dear Enginner
LM5118 is using unifunction current limit function at UPS.
Vin : 52 ~ 56, Vout(Battery cell) : 39 ~ 54V @ 3A
In the initial operation, it varies from 2.9A to about 1A, causing ocsillation.
As temperature of IC increases, damag is continuing.
It has continuously attempted to change the webench results and external compent, but has not improved.
so, I would like to inquire about how to make improvements or if there are any other recommendation IC.
Thanks.