Other Parts Discussed in Thread: BQ76930
I use bq76930 AFE and cell connection is 7cells.
VC0-VC1: CELL1
VC1-VC2: CELL2
VC2-VC3: CELL3
VC3-VC4: short
VC4-VC5: CELL4
VC5-VC6: CELL5
VC6-VC7: CELL6
VC7-VC8: short
VC8-VC8: short
VC9-VC10: CELL7
As described at datasheet,
The host controller must ensure that no two adjacent cells are balanced simultaneously
within each set of the following:
VC1–VC5
VC6–VC10
For 7cells connection,
CELL3 and CELL4 is adjacent? Can I enabled cell balance of CELL3 and CELL4 simultaneously?
CELL6 and CELL7 is adjacent?
Thanks