This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Leakage current from Input to output

Other Parts Discussed in Thread: DCR021205

What is the leakage current from input to output of DCR021205? See attached other manufaturer spec for ref

  • There  is no continuous leakage  current test for  the DCR021205 . The input to output wire capacitance is typically 25pf.There are no additional components between primary and secondary windings.

    The product is limited to:

     

    The external continuous voltage difference limits are defined as voltages as measured between VIN (-) and Vout (-) ground). The converter is designed as ground fault isolation device. It is not designed to operate with a continuous voltage isolation barrier at greater than 60VDC. The isolation 1 second test validates only the magnetic coating separation between primary and secondary transformer wire.

    tom