Other Parts Discussed in Thread: BQ25606
Hi,
I just created a discussion in the Battery Charger forum, but I think it's more suited here.
We are testing a prototype which runs on batteries and can be charged with USB. The charger is a BQ25606, and the buck-boost is a TPS63070.
Everything worked well, the battery charger worked and the circuit was stable. But at one time, we plugged the USB for 20 minutes (not the first time that we do so), and then the circuit stopped working.
I cut the trace between V_CHARGER_OUT and the VIN of the TPS63070, plugged 4V (from a power supply) directly to the input of the TPS, and there was clearly a short (500 mA consumed, which was the limit of the power supply).
I then applied 3.3V to the output of the TPS63070, and the circuit operated normally. So I really think that the TPS63070 is burned. Moreover, I did an Ohm test between VIN of the TPS63070 and GND and I measured 7 Ohms.
Does anyone have an idea about what happened? We did plug the USB before without problems for long periods.