This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM46002: Differences between the efficiency and the efficiency (log-scale) chart

Part Number: LM46002

Tool/software: WEBENCH® Design Tools

Hello together,

today I used the TI Webench to design an switchting regulator. The frame conditions are: V_in=10...50 V, V_out=3.3 V and I_out=2 A. Webench proposed me to use the LM46002 if I want to have also a good efficiency under low current conditions. In the following I plotted the charts for efficiency (log-scale) and efficiency, but I don't understand why I get a minima on the left chart @0.27 A, that doesn't occure on the right chart. 

Has anyone an idea why I get this result? In my opinion, it can only be a mistake in the calculation of the diagrams or an inaccuracy occurring there.

Thanks for your help and sorry for my bad English

Max