Other Parts Discussed in Thread: TIDA-00628, UCC28730, UCC24650, UCC28700-Q1, UCC28910
Hi,
We got a question from the customer about UCC28730-Q1.
Could you help us?
[Question]
They are considering designing non-Isolated Flybuck with UCC28730-Q1 based on TIDA-00628.
Vin=DC400~500V
Vout1=15V
Vout2=7V
Iout1=300mA
Iout2=100mA
Regarding the design with UCC28730-Q1 based on TIDA-00628, are there any concerns for that? If there is similar design of this, could you provide us?
Best Regards,
tateo