This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

advice on bit addressable

Other Parts Discussed in Thread: MSP430F135, MSP430F1101

1)I have some basic doubts. How can i access each pins of PORTS on MSP430F135. Allthough i remember reading the PORTS to be bit addressable. The above task is imperative coz in i have got three output on the same port. when i try to output the first , the second and the third should not get affected.
2) the code below runs absolutely fine on the IAR debugger. I have an LED connected on P2.2. According to the code, it should toggle everytime the TRANSMIT routine is called. But it doesnt happen. I dont know where i am gng wrong.
Please advice on both issues.

;*******************************************************************************
        .cdecls C,LIST,"msp430f1101.h"; Include device header file
;*******************************************************************************
        .data                    ;defining variables
;*******************************************************************************
 
CLOCK        .equ        020h                ;P1.5 CLOCK
STROBE        .equ        080h                ;P1.7 STROBE
DATA        .equ        R4                ;contains a bye to be transfered serially
;*********************************************************************************
        .text                    ;Program Start
;*******************************************************************************
RESET        mov.w   #200h,SP                ; Initialize stackpointer
STOPWDT         mov.w   #WDTPW+WDTHOLD,&WDTCTL  ; Stop WDT
CLEARP1            bic.b   #000h,&P1OUT            ; Clearing all the port pins
SETUPP1        mov.b    #0E0h,&P1DIR            ; CLOCK, STROBE, P1.6 as output
SETUPP2         mov.b   #004h,&P2DIR                ; P2.2 LED as output
SETUP        mov.b    #002h,&P1DIR            ; P1.1 LED as output
        mov.w    #040h,DATA                ; predefined data     
             
             
REPEAT        call     #TRANSMIT     
        jmp     REPEAT
;******************************************************************************
TRANSMIT                ;shifting data out serially to 4094
;******************************************************************************
        push.b  DATA                    ; TOS = Save Data
                mov.b   #040h, R5
TX_loop            mov.b    R5,&P1OUT
CLOCK_1        bis.b   #CLOCK,&P1OUT           ; Clock Pulse On Period
CLOCK_0         bic.b   #CLOCK,&P1OUT           ; Clock Pulse Off Period
STROBE_1    bis.b   #STROBE,&P1OUT          ; Strobe Pulse On Period
STROBE_0    bic.b   #STROBE,&P1OUT          ; Strobe Pulse Off Period
        xor.b    #04h,&P2OUT
        pop.b   DATA                    ; Original data
                ret                             ; Return from subroutine
                                                         
***********************************************************************************
;           Interrupt Vectors
;***********************************************************************************
            .sect   ".reset"                ; MSP430 RESET Vector
            .short  RESET                   
            .end