This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92641: TPS92641 current issue

Part Number: TPS92641

Dear,

My customer is using TPS92641 to control 500 LED lamps, string 10 together as a string, and connect 50 string in parallel.

Each of lamps need 3V@120mA, so the total current is 5A needed, but the total current is around 900mA now. 

Please help to check.

The system input is 48v,output is 35V@6A, MOSFET is PSMN069_100YS