When I used UCD3xxx Device GUI with UCD3020, I encountered a problem.
I want to use memory debugger, but when I clicked the memory debugger after clicking Device ID, a warning window appeared.
The information in the window :
This feature is not available in program (flash) mode on the EVMPSFB00 @ 88d. The device does not support the PARM_INFO and PARM_VALUE commands. These commands are used to peek/poke memory when the IC is in program (flash) mode. Please review your command bitmask or contact TI for asistance.