Other Parts Discussed in Thread: CC2640R2F, , BOOSTXL-BATPAKMKII
Hi,
My setup is CC2640R2F Launchpad + BOOSTXL-BATPAKMKII with BQ27441-G1. Here are my battery information below. If I multiply the Design Capacity 1200 mAh with State OF Charge 98%, the result is 1176 mAh. But from the battery information below, the remaining capacity is 1066mAh. There is 110 difference. How did the State Of Charge became 98%?
*************************************
Battery Information
*************************************
Design Capacity: 1200mAh
Remaining Capacity: 1066mAh
State of Charge: 98%
Temperature: 30C
Voltage: 4111mV
Average Current: -28mA
Status : discharging
-kel