I am a little confused about the values that should be used for the COMM1 to AC1 and COMM2 to AC2 for the Communication Modulator on the bq51050b.
- Section 8.3.4.8 of the bq5105xB data sheet indicates a 47nF capacitor should be used for each (for a total of about 22nF)
- SLUUA25C (bq51050BEVM-764) uses a 22nf Capacitor for each
- Which value should I use?
- How critical are these capacitor values?