This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: I am having difficulty calibrating/configuring a new build and would like some assistance.

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQSTUDIO

I am working with a 4s1p 3.2Ah battery pack with the bq40z50r2 solution.  I am trying to get some samples ready for our customer to test out. 

Given the difficulty and complexity doing simple things we used to do rather easily before, I am almost regretting the choice to go with this device.

When the pack is connected to bqStudio, after calibration the cell voltages are not reported correctly.  Cell 1 is always several hundred mv less than cells 2-4.

After cc offset calibration, cell current is non-zero and I cannot calibrate board offset.

If you reach out I can provide the schematic and more details.

Thanks,

Joe Perino

GM, Nova Battery Systems