Other Parts Discussed in Thread: GPCRB
Hi,
I use the BQ27542-G1 in the battery pack, there're some abnormal problems in the low temperature test: -20'C, 300mA, discharge:
1. When has been discharge into the cut-off voltage, SOH value is reduced, can return to 100%.
2. But if you stop in the middle of the low temperature discharge, SOH value will reduce, and can't come back. even if let it stand for awhile at room temperature, it won't recover.
3. 100% of the battery SOC, the SOH 100% change into 98%.
let it stand for awhile at room temperature, the SOH is still 98%. it can't recover to 100%.
discharge to 0% , then confirm SOH 98% change into 100%, it's recoverable.
4. Using 50% battery SOC at low temperatures -20'C, 300 mA, discharge, there's no SOH change phenomenon.
Now the SOH failure rate is 100%, and I don't know the problem itself is normal or abnormal phenomenon. How to solve it ?